AXIS#.BODE.FREQ
Description
AXIS#.BODE.FREQ sets the frequency of the sine excitation source in Hz. The sine excitation source is used to take frequency response measurements of a system.
Example
Setting up a sine excitation source of 0.2 A at 50 Hz:
-->AXIS1.BODE.INJECTPOINT 1
-->AXIS1.BODE.IAMP 0.2
-->AXIS1.BODE.FREQ 50.0
-->AXIS1.BODE.MODE 2
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
|
Type |
Read/Write |
|
Units |
Hz |
|
Range |
0 to 8,000 Hz |
|
Default Value |
0 Hz |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Related Topics
Using the Performance Servo Tuner
Using the Performance Servo Tuner: Advanced
|
Copyright © 2018 Kollmorgen |
|